Similar to the portable swaging tool the
cutter tool is easy to use and requires only a
hand wrench.
The first step is to tighten the face
support and the cutter support onto the bearing
so that the ball and outer race are locked in
place.
The washers will insure that the cutter
maintains constant pressure.
A wrench is then applied to the hex of the
cutter and rotated to cut the retention groove
flange. An internal stop on the cutter will
keep the cutter teeth from penetrating into and
damaging the housing.